Start main contents

  • Register
  • Login

Factory Automation

Print page

Factory Automation

Products and Solutions

Solutions

Show all

Products

2019-04-10
Mitsubishi Electric launches HMI for extreme environments - With an extended operating temperature range of -20°C to +65°C, and protection ratings to IP67F/IP66F, the GOT2507T-WTSD 7” operator terminal meets the needs of harsh and demanding applications. No additional protective measures are required for washdown with high pressure water or use in power equipment that is typically located outdoors. As a result, it is a perfect fit...
2019-04-01
New performance inverters for applications with high power requirements - Mitsubishi Electric has extended its inverter portfolio with a 690V version of its FR-A800 series inverters. The new models of the FR-A870 690V line cover power outputs up to 1.5 MW. Yet this increased power is delivered in a slim package that starts at just 380mm wide, offering significant space saving potential. Furthermore, the FR-A870 line combines this high-power performance with features ...
2019-01-08
New benchmark SCADA software platform - MAPS 4, the latest SCADA solution from Mitsubishi Electric for control and visualisation, extends connectivity options, adds user tools and increases the scope of its built-in functionality. The result is a software suite that can reduce the time taken for project development and integration, while also enabling users to realise Smart Factory objectives.
2018-11-29
Automation trends in the packaging industry - Like many other industries, the packaging sector constantly adapts to market requirements. Changes are being influenced by factors such as regulation, skills shortages and digital transformation. To turn these challenges into opportunities, innovative companies are increasingly relying on solutions such as human-robot collaboration and the use of artificial intelligence to ...
2018-11-28
How to achieve faster SCADA projects - Within the myriad of possible applications for SCADA software there is a common theme for both the end user and system integrator, and that is a need to respond to competitive pressures. The reason manufacturing, process, logistics and utility businesses all invest in new control and monitoring software is to build more efficient, cost-effective operations.

Show all


Guided Operator Solutions (Poka Yoke) – Mitsubishi Electric's lean strategy for human mistake prevention. Eliminating mistakes in manufacturing or logistics operations at the source.
More info

Mitsubishi Electric HMI Migration Guide – After many years of success, Mitsubishi Electric are replacing their E1000 HMIs with a new range of HMIs called GOT2000 which incorporate newer technologies and offer significant benefits.
Download it here

Contact Image Sensors – Highest image quality with minimum effort
CIS
Page top