• Register
  • Login

Factory Automation

Print page

Products and Solutions



2018-01-16New widescreen operator interfaces offer more comfortable machine handling - Mitsubishi Electric has expanded its GOT2000 series of Human-Machine Interfaces (HMI) with two new widescreen versions. The ability to display additional visual information gives users of the new GT21 and GT25 widescreen HMIs the opportunity to enhance machine operability and the potential to increase productivity. Other valuable features include two separate Ethernet ports and ...More
2017-11-29Quality management and digitalisation in manual assembly operations - At SPS IPC Drives 2017, Mitsubishi Electric’s Guided Operator Solutions for manual assembly applications will demonstrate how improvements in quality and productivity can be achieved. These solutions also enable the seamless transfer of production data from manual assembly operations to higher-level enterprise systems, supporting the digital transformation within manufacturing.More
2017-11-29Mitsubishi Electric previews extension to its range with collaborative robot - Supporting humans with a full complement of robot features and equipment on board At SPS IPC Drives from 28 - 30 November 2017 in Nuremberg, Mitsubishi Electric is setting up a demonstration of production in an Industry 4.0 environment that will include a new collaborative robot, working together with an operator without safety barriers. More
2017-11-28Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages - Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.More
2017-05-05Key technology supporting packaging applications on their journey to Industry 4.0 - Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017. More
2012-05-08More productivity and efficiency – Mitsubishi's new RH-F series is a range of robust, high-quality robots with an outstanding price/performance ratio. They are suitable straight from the factory for a wide range of industrial applications and can be deployed in many industries.More
2012-03-15The rack-free modular controller: MELSEC L Series – MELSEC L series is a powerful but compact modular controller with many features built-in to the CPU itself. With its excellent cost performance and usability it is ideal for use in mid-size control applications.More
2011-12-13The machine builder's HMI – With the GT14 Mitsubishi Electric has enhanced its GOT1000 series of graphic operation terminals. The GT14 sets new performance benchmarks for mid-range 5.7” panel-mount terminals.More
Knowledge Base

Guided Operator Solutions (Poka Yoke) – Mitsubishi Electric's lean strategy for human mistake prevention. Eliminating mistakes in manufacturing or logistics operations at the source.
More info

Mitsubishi Electric HMI Migration Guide – After many years of success, Mitsubishi Electric are replacing their E1000 HMIs with a new range of HMIs called GOT2000 which incorporate newer technologies and offer significant benefits.
Download it here

Contact Image Sensors – Highest image quality with minimum effort